Module Use in Applications (Zone Damper) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Zone Damper Uses in Application System Selection Trees

Module Instance Name

Applications

Zone X Damper Control v50 (Where X is 1-8)

AHU Multizone (Mixed Air Dual Duct) Applications

To see a module's connections and how modules interact with it, view the Connections table.