Attributes (Heating Staged Outputs with DA-T Low Limit) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18
Language
English

The following table describes the attributes used by the Heating Staged Outputs with DA-T Low Limit module.

Table 1. Heating Staged Outputs with DA-T Low Limit Attributes

Name

Type 1

Description

Default Value

Control Band

V

Control band for the MSC.

Display Units: °C

Control Status

V

Current status of the controller for heating control.

Set Name: Control Status

Eff Minimum Off Time

V

Minimum off time used by the MSC.

Display Units: Seconds

Eff Minimum On Time

V

Minimum on time used by the MSC.

Display Units: Seconds

Eff Process Time Const

V

Contains the effective process time constant used by the MSC.

Display Units: Seconds

Eff Process Variable

V

Process Variable used by the MSC.

Display Units: °C

Failsoft Value

 

Contains the value of the output when the mode is Failsoft.

0.0%

HTG-ABSEFFORT (Heating Absolute EWMA Effort)

 

Provides an EWMA based on the absolute value of (Current Present Value - Last Present Value). The PID computes this value.

0.0

Display Units: %

HTG-ABSERROR (Heating Absolute EWMA Error)

 

Provides an EWMA based on the absolute value of (Setpoint - Process Variable). The PID computes this value.

0.0

Display Units: °C, °F

HTG-ERROR (Heating EWMA Error)

 

Provides an EWMA based on the difference of (Setpoint - Process Variable). The PID computes this value.

0.0

Display Units: °C, °F

HTG-EWMA (Heating EWMA Present Value)

 

Provides an EWMA of the Present Value. The PID computes this value.

0.0

Display Units: %

HTG-MINOFF (Minimum Off Time)

 

Contains the Min Off Duration for all stages.

120 Seconds

HTG-MINON (Minimum On Time)

 

Contains the Min On Duration for all stages.

120 Seconds

HTG-O (Percent Cmd)

V

Contains a representative analog percent output on a scale of 0% to 100%.

Display Units: %

HTG-OUTSTATE (State)

V, G

Current operational mode of the output controller.

Set Name: UV Discrete Out

Instant Shutdown

V

Contains the indication to the MSC to shut all outputs off instantly.

 

Limited Max Value

 

Specifies that when the mode is set to Limited Max, the output cycles to maintain this percentage duty cycle.

100.0%

Low Limit Process Variable

 

Contains the process variable controlled when the mode is set to Control Limit. This value typically is connected to the Discharge Air Temperature.

13 °C, 55 °F

Low Limit Setpoint

 

Contains the desired setpoint for the low limit process variable to be controlled to when the mode is Control Limit.

13 °C, 55 °F

Max Capacity Fraction

 

Contains the ratio of the largest stage to the sum of all the stages.

1.0

Mode

 

Mode requested by State Selection.

Off

Set Name: UV Discrete Out

Output Overridden

 

Indicates when the actual output controlled by this output is overridden by a user.

False

Output Position

 

Provides the current Present Value of the output that this controller drives.

0%

PID Tuning Reset

 

Causes the PID objects to reset their tuning parameters to the default based on the appropriate Process ID.

Normal

Set Name: PID Tuning Reset

PMAC Period

V

Specifies the period used by the PMAC algorithm portion of the MSC.

Display Units: Seconds

Process Units

 

Specifies the units for the PID. For this particular module, °C and °F are the only two valid values.

°C

Set Name: Unit

Process Variable

 

Specifies that when the mode is set to Control, this is the variable that is controlled. This value typically is connected to the Zone Temperature.

22 °C, 72 °F

Proof of Airflow

 

Specifies that when set to False or True, the controller operates as normal. When set to Fault, the controller transitions to an instant off state.

True

Set Name: False/True/Fault

Setpoint

 

Desired setpoint for the process variable to be controlled to when the mode is set to Control.

22 °C, 72 °F

1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)