Reliability (Heating Proportional Valve with Low Limit) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
Table 1. Heating Proportional Valve with Low Limit Reliability

Input

Behavior When Input Is Not Reliable

Low Limit Process Variable

If the requested mode is Remain In Control, the output controller changes to Failsoft.

OA Temperature

If the requested mode is Low OA Temperature, the output controller changes to Failsoft.