Reliability (Heating FBPD Proportional Valve with Low Limit) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18
Table 1. Heating FBPD Proportional Valve with Low Limit Reliability

Input

Behavior When Input Is Not Reliable

OA Temperature

If the requested mode is Low OA Temperature, the output controller changes to Failsoft Valve.

Low Limit Process Variable

If the requested mode is Remain In Control, the output controller changes to Failsoft Valve.