Module Use in Applications (Heat Pump Staged Compressors) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Heat Pump Staged Compressors Uses in Application System Selection Trees

Module Instance Name

Applications

Staged Compressor Control v51

Heat Pump Applications

To see a module's connections and how modules interact with it, view the Connections table.