Module Use in Applications (Cooling Staged Outputs) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Cooling Staged Outputs Uses in Application System Selection Trees

Module Instance Name

Applications

Staged Cooling Control v51

Fan Coil Applications

Unit Ventilator Applications

To see a module's connections and how modules interact with it, view the Connections table.