Module Use in Applications (Cooling Proportional Valve with Dehumidification) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Cooling Proportional Valve with Dehumidification Uses in Application System Selection Trees

Module Instance Name

Applications

Proportional Valve Cooling Control v51

All

To see a module's connections and how modules interact with it, view the Connections table.