Attributes (Single Speed Fan Control) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18
Language
English

The following table describes the attributes used by the Single Speed Fan Control modules.

Table 1. Single Speed Fan Control Attributes

Name

Type 1

Description

Default Value

Fan OnOff

 

Contains the output command enumeration for information feedback representing the on/off status of the fan.

Set Name: Off/On

Mode

 

Mode requested by State Selection.

Off

Set Name: Off/On

1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)