Module Use in Applications (Parallel Fan Control) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Parallel Fan Control Uses in Application System Selection Trees

Module Instance Name

Applications

Parallel Fan Control

VAV Single Duct Applications

To see a module's connections and how modules interact with it, view the Connections table.