Attributes (Parallel Fan Control) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18
Language
English

The following table describes the attributes used by the Parallel Fan Control modules.

Table 1. Parallel Fan Control Attributes

Name

Type

Description

Default Value

Input

 

The input to the pass through module

Off

Set Name: Off/On

Present Value

G, V

The output of the pass through module

Set Name: Off/On