Fan Proportional - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

This module controls a proportional fan. The module accepts as inputs a command, a heating percentage and a cooling percentage. Based upon the input command and parameter settings, the module outputs a percent command and an on/off command.

You can view and modify the modules in this group’s logic.