Module Use in Applications (Fan Supply Duct Static Control) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18
Language
English

The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Fan Supply Duct Static Control Uses in Application System Selection Trees

Module Instance Name

Applications

Variable Capacity Supply Fan Control

AHU Mixed Air Single Duct Applications

AHU Mixed Air Dual Duct Applications

AHU 100% Outdoor Air Single Duct Applications

AHU 100% Outdoor Air Dual Duct Applications

To see a module's connections and how modules interact with it, view the Connections table.