Module Use in Applications (Fan Single Speed) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Fan Single Speed Uses in Application System Selection Trees

Module Instance Name

Applications

Constant Capacity Exhaust Fan Control

AHU 100% Outdoor Air Single Duct Applications

AHU 100% Outdoor Air Dual Duct Applications

Constant Capacity Return Fan Control

AHU Mixed Air Single Duct Applications

AHU Mixed Air Dual Duct Applications

AHU Multizone (Mixed Air Dual Duct) Applications

Constant Capacity Supply Fan Control

All

To see a module's connections and how modules interact with it, view the Connections table.