Attributes (Fan Single Speed) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
The following table describes the attributes used by the Fan Single Speed modules.

Table 1. Fan Single Speed Attributes

Name

Type 1

Description

Default Value

Fan OnOff

 

Contains the output command enumeration for information feedback representing the on/off status of the fan.

Set Name: Off/On

FAN-OUTSTATE (State)

 

Current operational state of the output controller.

Set Name: Off/On/Hold

Mode

 

Mode requested by State Selection.

Off

Set Name: Off/On/Hold

1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)