Module Use in Applications (Fan Return or Exhaust Tracking) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Fan Return or Exhaust Tracking Uses in Application System Selection Trees

Module Instance Name

Applications

Variable Capacity Exhaust Fan Track Control

AHU 100% Outdoor Air Single Duct Applications

AHU 100% Outdoor Air Dual Duct Applications

Variable Capacity Return Fan Track Control

AHU Mixed Air Single Duct Applications

AHU Mixed Air Dual Duct Applications

To see a module's connections and how modules interact with it, view the Connections table.