The Zone Damper Limit Control uses the feedback of the Percent Cmd to begin controlling at the current damper position, when either form of limit control is required to maintain the discharge air temperature. When the transition out of a limit control occurs, the UV Zone Damper Control is already in control or the state requested is a fixed position state and does not require the Percent Cmd as its startup value.