Module Use in Applications (Exhaust Damper Control) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Exhaust Damper Control Uses in Application System Selection Trees

Module Instance Name

Applications

Exhaust Damper Control v102

All

To see a module's connections and how modules interact with it, view the Connections table.