Module Use in Applications (Min OA Damper Proportional Output) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
The application System Selection trees use the individual modules in this group using the name in the following table.

Table 1. Min OA Damper Proportional Output Uses in Application System Selection Trees

Module Instance Name

Applications

Proportional Damper Minimum OA Flow Control

AHU Mixed Air Single Duct Applications

AHU Mixed Air Dual Duct Applications

To see a module's connections and how modules interact with it, view the Connections table.