Module Use in Applications (VF Primary Min Flow Control) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18
Language
English

The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. VF Primary Min Flow Control Uses in Application System Selection Trees

Module Instance Name

Application

CHW Pump Differential Pressure Control

Central Cooling with Optimization Applications

HW Pump Differential Pressure Control

Central Heating Applications

Primary CHW Bypass Valve Control

Central Cooling with Optimization Applications

VF Primary Min Flow Control

Central Cooling with Optimization Applications

To see a module's connections and how modules interact with it, view the Connections table.