Primary States (Tower Control) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18
Language
English
  • Off: Turn the device off. Set the Output to 0%, set the Alarm to Off, delay off the interlock Command, and set the Command to Off.

  • On: Enable the inputs to start and stop the device.