Sequenced Output - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The Sequenced Output module takes one proportional output and spans it over two proportional outputs. This module accepts as inputs an Input (float) and a Valve 1 Percent Capacity. Based on the input commands, the module outputs two proportional outputs.

You can view and modify the modules in this group’s logic.