Attributes (Ramp to Command with Limit) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
The following table describes the attributes used by the Ramp to Command with Limit modules:

Table 1. Ramp to Command with Limit Attributes

Attribute

Type 1

Description

Default Value

Command

 

Provides the command to the device.

Off

Set Name: Off/On

Min Speed

 

Indicates the minimum value of the Percent Command when the Percent Cmd is 0.0%.

0.0%

Percent Cmd

 

Indicates the value from the PID module. It provides the control signal for the VFD outputs.

0.0%

Percent Command

V

Indicates the percent command that is being sent to the VFD for the pump.

0.0%

Percent Limit

 

Indicates the value that limits the maximum output of the module.

100.0%

Ramp Time

 

Indicates the time (in minutes) for the module to ramp from zero to the minimum of the Percent Limit and the Percent Cmd on startup.

5.0 Minutes

State

G, V

Indicates the current state of the activity.

Default Value: Off

Set Name: CP Pump Output Control

System Enable

 

Indicates whether the system is enabled.

True

1 B - BACnet Exposed Parameter, C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)