Attributes (Pump Startup Determination) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
The following table describes the attributes used by the Pump Startup Determination modules:

Table 1. Pump Startup Determination Attributes

Attribute

Type 1

Description

Default Value

Device nn Status

 

Indicates whether any of the pumps should be turned on. This module has 8 inputs.

False

Output

G

Indicates that one or more pumps should start. The output is an Or function of the inputs.

False

1 B - BACnet Exposed Parameter, C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)