The application System Selection trees use the individual modules in this group using the names in the following table.
Module Instance Name |
Applications |
---|---|
CWP Selector XX (Where XX Is 01-08) |
|
PCHWP Selector XX (Where XX Is 01-08) |
|
Pump Selector XX (Where XX Is 01-08) |
|
SCHWP Selector XX (Where XX Is 01-08) |
To see a module's connections and how modules interact with it, view the Connections table.