Primary States (Pump Output Control) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
  • Off: Sets the Device OnOff output to off. The Percent Command is set to 0%.

  • On: Sets the Device OnOff output to on. The Percent Cmd is set to 100%.

  • Control: Sets the Device OnOff to on. When this state is first entered a Rate Limit object begins to increase its output starting from zero. When the output of the rate limit reaches the minimum of the Percent Cmd input and the Percent Limit input, the minimum of those two inputs is passed to the Percent Command output. The Percent Command varies between Min Speed and 100% as the input Percent Cmd varies from 0 to 100%.

  • Hold: Holds the Device OnOff and Percent Command at the last outputed value.

Figure 1. Pump Output Control Signal Relationships During Control

Table 1. PMP Control Command Hierarchy (Enum Output)

System Enable

Enable

Blocking Protect

Command

Speed Setting

State

FALSE

*

*

*

*

Off

TRUE

FALSE

*

*

*

Off

TRUE

TRUE

Protect

*

*

On

TRUE

TRUE

Off

FALSE

*

Off

TRUE

TRUE

Off

TRUE

Variable Capacity

Control

TRUE

TRUE

Off

TRUE

Constant Capacity

On