Module Use in Applications (Pump Output Control) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
The application System Selection Trees use the individual modules in this group using the names in the following table.

Table 1. Pump Output Control Uses in Application System Selection Trees

Module Instance Name

Application

CW Pmp X Control (Where X Is 1-8)

Central Cooling with Optimization Applications

CHW Pump X Control (Where X Is 1-8)

Central Cooling with Optimization Applications

Secondary Pump X Control (Where X Is 1-8)

Central Cooling with Optimization Applications

To see a module's connections and how modules interact with it, view the Connections table.