Pump Output Control - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
The Pump Output Control module provides proper operation of a constant speed or variable speed pump. It provides the on/off signal to turn on both variable speed and constant speed pumps. This module also provides the variable output signal for a variable speed pump. Based on the Mode input, it sets the Device OnOff output and the Percent Command Output. This module is implemented as a hybrid control activity.

You can view and modify the modules in this group’s logic.