Module Use in Applications (Open Loop Tower Control with Low Limit) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Open Loop Tower Control with Low Limit Uses in Application System Selection Trees

Module Instance Name

Applications

Open Loop Tower Control with Low Limit

Central Cooling with Optimization Applications

To see a module's connections and how modules interact with it, view the Connections table.