Attributes (Damper Command OR) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18
Language
English

The following table describes the attributes used by this module.

Table 1. Damper Command OR Attributes
Attribute Type 1 Description Default Value
Device 1 Cmd   Represents the command being sent to the first device. Close
Device 2 Cmd   Represents the command being sent to the second device. Close
Present Value   Represents the result of the OR operation. Close
1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)