Module Use in Applications (Cooling Tower Speed Count Determination) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
The application System Selection Trees use the individual modules in this group using the names in the following table.

Table 1. Cooling Tower Speed Count Determination Uses in Application System Selection Trees

Module Instance Name

Application

Cooling Tower Speed Count Determination

Central Cooling with Optimization Applications

To see a module's connections and how modules interact with it, view the Connections table.