The Chiller Output Control module provides proper operation of a chiller and, when required by chiller plant configuration, its isolation valves. This module provides the on/off signal that enables a chiller to operate and provides open and close commands for a two position isolation valve. This module also provides the variable output signal for an analog isolation valve. Based on the Mode input, the module sets the Chiller OnOff, Iso Valve OpenClose, Iso Valve Pct Cmd, and Inputs and Outputs.
You can view and modify the modules in this group’s logic.