Module Use in Applications (Block Protect) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
The application System Selection Trees use the individual modules in this group using the names in the following table.

Table 1. Block Protect Uses in Application System Selection Trees

Module Instance Name

Applications

CHW Pump X Block Protect (Where X Is 1-8)

Central Cooling with Optimization Applications

CW Pump X Block Protect (Where X Is 1-8)

Central Cooling with Optimization Applications

Cooling Tower X Block Protect (Where X Is 1-8)

Central Cooling with Optimization Applications

Secondary Pump X Block Protect (Where X Is 1-8)

Central Cooling with Optimization Applications

To see a module's connections and how modules interact with it, view the Connections table.