Attributes (Block Protect) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18
Language
English

The following table describes the attributes used by the Block Protect modules:

Table 1. Block Protect Attributes

Name

Type 1

Description

Default Value

Blocking On Time

 

This input defines the duration of time to run the device.

5.0 Seconds

Command

 

This input represents the command being sent to the device.

Off

Set Name: Off/On

Max Off Time

 

This output defines the duration of time between run commands to the device. If set to zero, blocking protection is not performed.

7.0 Days

Min Value: 0

Max Value: 45

State

G

This output displays Protect when the Max Off Time is exceeded and Command is Off. The device remains in the Protect state until Blocking On Time is met or the Command input is changed to On.

Off

Set Name: Block Protect

Total Off Time

SC

This output indicates the amount of time spent in the Off state. When this value exceeds the Max Off Time input value the state switches to Run for the duration of the Blocking On Time.

Display Units: Days

1 B - BACnet Exposed Parameter, C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)