Module Use in Applications (Supply Flow Setpoint Control HFR) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
The application System Selection trees in the software use the individual modules in this group using the name in the following table.

Table 1. Supply Flow Setpoint Control HFR Uses in Application System Selection Trees

Module Instance Name

Applications

Supply Flow Setpoint Control HFR

VAV Single Duct Applications

To see a module's connections and how modules interact with it, view the Connections table.