Primary States (Subordinate Supply Flow Setpoint Control HFR) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18
Language
English
  • Min: Output the Cooling Min Flow Setpoint.

  • Max: Output the Cooling Max Flow Setpoint.

  • Hold: Maintain the current flow setpoint.

  • Control: Adjust the flow setpoint to maintain the process variable at the cooling setpoint. The flow setpoint adjusts between the minimum and maximum flows.

  • Heating: Set the flow setpoint to the value of the Heating Min Flow.

  • Warmup: Adjust the flow setpoint to maintain the process variable at the heating setpoint.

  • Failsoft: Output the flow setpoint that is spanned between the Cooling Min Flow and Cooling Max Flow by the value of the Failsoft Value (percent).

  • Heating Flow Reset: Increase the flow when the maximum heating output is reached.