Module Use in Applications (Flow Setpoint [VAV Dual Duct]) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The application System Selection trees in the software use the individual modules in this group using the names in the following table.

Table 1. Flow Setpoint (VAV Dual Duct) Uses in Application System Selection Trees

Module Instance Name

Applications

CD Constant Flow Setpoint Control v51

VAV Dual Duct Applications

CD Flow Setpoint Control v51

VAV Dual Duct Applications

HD Flow Setpoint Control v51

VAV Dual Duct Applications

Note: The Flow Setpoint (VAV Dual Duct) module instances appear in the Output Control category; however, to add a new Flow Setpoint (VAV Dual Duct) module from the palette (Module Selection dialog box), select New from the State Generation header right-click menu.

To see a module's connections and how modules interact with it, view the Connections table.