Network Output Modules - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18
Language
English

The Network Outputs module category appears in the Control View of the tool and lists the network outputs defined for the system. A Network Output allows an output to be connected to over the network, acting as a network variable read from a supervisory device. When a network output is not mapped to a supervisory device, it can only be viewed from the Commissioning mode of the tool. Network outputs connect from other modules or the State Table. The main difference between these outputs is the data type.

Network Output modules fall into one of the following categories:

Output Control Interface Modules

Central Plant Interconnection Modules

VAV Application Interconnection Modules

Generic (Add New) Modules

See also the N2 Compatibility Network Outputs section in N2 Compatibility Options.

See the Upgrading System Files section for a list and description of the module and System Selection changes that were made since the last release of the tool.