Key Sensor and Setpoint Network Inputs are created during System Selection to allow system-wide logic to easily interface with the local control logic.
Typical examples for sensors include scenarios when the Supervisory System provides Outdoor Air Temperature and Humidity values for all the local devices using Network Inputs. An example use is that a Supervisory device reads an Outdoor Air Temperature sensor from one device and writes its value to the network input of other devices.
Another example is that Subordinate VAV box applications read key values from the master VAV box applications using peer-to-peer references to make sure the zone under control does not have some VAV boxes calling for cooling while others are calling for heating.
The following table describes the Sensor and Setpoint Network Input modules and lists the applications in which they are used.
If you wish to change the default names used for these modules, you can do so by editing the Object Naming Preferences. See the following topics in the Setting Preferences section for details: Object Naming and Signal Preferences, Setting Default Naming and Signal Preferences, and Preferences - Naming and Signal.
Name |
Description |
Applications |
---|---|---|
BLDGP-SP |
Building Static Pressure Setpoint |
|
BLR-SP |
Boiler Setpoint |
|
BLRSTG-SP |
Boiler Stage-up Setpoint |
|
CD-OA% |
CD OA Percent |
|
CDT-SP |
Cold Deck Air Temperature Setpoint |
|
CH-SP |
Chiller Setpoint |
|
CHW Coil X Percent Cmd (Where X Is 1-4) |
CHW Coil X Percent Cmd |
|
CHWDP-SP |
CHW Differential Pressure Setpoint |
|
CHWDT-SP |
Differential Temperature Chill Water Setpoint |
|
CLGOATLOCKOUT-SP |
OA Cooling Enable Setpoint |
|
CLGUNOCC-SP |
Night Cooling Setpoint |
|
CP X Runtime Reset (Where X is 1 or 2) | CP 1 Runtime Reset, CP 2 Runtime Reset | |
CTSTG-SP |
CT StageUp Setpoint |
|
CT-MINOFF |
Cooling Tower Minimum Off Time |
|
CT-MINON |
Cooling Tower Minimum On Time |
|
CW-SP |
Condenser Water Setpoint |
|
CWDP-SP |
CW Differential Pressure Setpoint |
|
CWDT-SP |
CW Differential Temp Setpoint |
|
CW VFD Ramp Time |
CW VFD Ramp Time |
|
DAP-SP |
Duct Static Pressure Setpoint |
|
DATLL-SP |
Discharge Air Low Limit Setpoint |
|
DAT-SP |
Discharge Air Temperature Setpoint |
|
DCPLF-SP |
Decouple Loop Flow Setpoint |
|
DEHUM-SP |
Dehumidification Setpoint NI |
|
EAT-SP |
Exhaust Air Temperature Setpoint |
|
EFSTG-SP |
Exhaust Fan Stageup Setpoint |
|
FAN-RESET |
Fan Alarm Reset |
|
FBPD-SWO |
Network Switchover |
|
FLOW-DIFF |
Flow Differential Setpoint |
|
FLOW-LL |
Airflow Low Limit |
|
FLUSHPOS |
Flush Position |
|
FROST-DIFF |
Frost Protect Differential |
|
FROST-SPX (Where X Is 1-2) |
Frost Protect OA Setpoint X |
|
FSCS-EF |
FSCS Exhaust Fan |
|
FSCS-RF |
FSCS Return Fan |
|
FSCS-RLF |
FSCS Relief Fan |
|
FSCS-SF |
FSCS Supply Fan |
|
HCP X Runtime Reset (Where X is 1 or 2) | HCP 1 Runtime Reset, HCP 2 Runtime Reset | |
HD-OA% |
HD OA Percent |
|
HDT-SP |
Hot Deck Air Temperature Setpoint |
|
HTGOATLOCKOUT-SP |
OA Heating Enable Setpoint |
|
HTGUNOCC-SP |
Night Heating Setpoint |
|
HUM-SP |
Humidification Setpoint NI |
|
HWDP-SP |
HW Differential Pressure Setpoint |
|
HWFLOW-SP |
HW Min Flow Setpoint |
|
HWLO-SP |
HW Low Setpoint |
|
HWTHI-SP |
Hot Water Supply Temperature High Reset Temperature Output Range High |
|
HWTLO-SP |
Hot Water Supply Temperature Low Reset Temperature Output Range Low |
|
HWT-OARSTA |
Hot Water Supply Temperature Setpoint Reset Input Range Low |
|
HWT-OARSTB |
Hot Water Supply Temperature Setpoint Reset Input Range High |
|
HXSTG-SP |
Heat Exchanger Stage-up Setpoint |
|
ISOVLV-RT |
Chlr IsoVlv Ramp Time |
|
MAT-SP |
MA Temperature Setpoint |
|
MOADPOS-SP |
Min OA Damper Position |
|
MOAFLOW-SP |
Min OA Flow Setpoint |
|
MSTCDFLOW-OUTSTATE |
Master CD Constant Flow Setpoint Control |
|
MSTCDFLOW-OUTSTATE |
Master CD Flow Setpoint Control |
|
MSTHDFLOW-OUTSTATE |
Master HD Flow Setpoint Control |
|
MSTRCDFLOW-PERCENT |
Master CD Flow Percent |
|
MSTRFAN-C |
Master Fan Command |
|
MSTRFAN-O |
Master Fan Output |
|
MSTRFLOW-PERCENT |
Master Supply Flow Percent |
|
MSTRFLOW-S |
Master Flow Setpoint Status |
|
MSTRHDFLOW-PERCENT |
Master HD Flow Percent |
|
MSTRHTG-1C |
Master Heating Stage 1 Cmd |
|
MSTRHTG-2C |
Master Heating Stage 2 Cmd |
|
MSTRHTG-3C |
Master Heating Stage 3 Cmd |
|
MSTRHTG-C |
Master Heating Command |
|
MSTRHTG-O |
Master Heating Output |
|
MSTRSUPHTG- CMSTRSUPHTG1-C |
Master Supp Heating Command Master Supp Heating Stage 1 Cmd |
|
MSTRSUPHTG-O |
Master Supp Heating Output |
|
MSTRZN-CO2 |
Master Zone CO2 |
|
OAD-MINPOS |
OA Damper Minimum Position |
|
OA-H |
Outdoor Air Humidity |
|
OALT-SP |
OA Low Limit SP |
|
OA-PERCENT |
OA Percent |
|
OA-T |
Outdoor Air Temperature |
All Applications (except VAV Subordinate Applications) |
OCCFLOW-DIFF |
Occupied Flow Differential Setpoint |
|
PCHWP VFD Ramp Time |
PCHWP VFD Ramp Time |
|
PHP X Runtime Reset (Where X is 1 or 2) | PHP 1 Runtime Reset, PHP 2 Runtime Reset | |
PHP-ROT | Preheat Pump Rotate Now | |
Pump Delay |
Pump Delay |
|
RAT-SP |
Return Air Temperature Setpoint |
|
RFSTG-SP |
Return Fan Stageup Setpoint |
|
Relief Fan Stageup Setpoint |
||
RHP X Runtime Reset (Where X is 1 or 2) | RHP 1 Runtime Reset, RHP 2 Runtime Reset | |
RHP-ROT | Reheat Pump Rotate Now | |
SA-T |
Supply Air Temperature |
|
SCHWPSTG-SP |
Secondary Chill Water Stageup Setpoint |
|
SCHWP VFD Ramp Time |
SCHWP VFD Ramp Time |
|
SFSTG-SP |
Supply Fan Stageup Setpoint |
|
SHWPSTG-SP |
Stageup Setpoint |
|
SLH-SP |
Sideloop Humidity Setpoint |
|
SLP-SP |
Sideloop Pressure Setpoint |
|
SLT-SP |
Sideloop Temperature Setpoint |
|
STAGE-CAP |
Stage Capacity |
|
Stage Capacity (%FLA) |
||
Stage Capacity (AMPS) |
||
STMP-SP |
Setpoint |
|
UNIT-RESET |
Unit Reset |
|
UNOCCFLOW-DIFF |
Unoccupied Flow Differential Setpoint |
|
ZN-H |
Zone Humidity |
|
ZN-T |
Zone Temperature |
|
ZNT-SP |
Common Setpoint Zone Temperature Setpoint |
|
ZNX-SP |
Zone X Common Setpoint (where X is 1-8) |
|
Zone X Temperature Setpoint (where X is 1-8) |
||
ZONE-DIFF |
Zone Differential |