Generator Interface Modules - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18
Language
English

The Generator Interface Network Inputs are always paired with a State Generation module. These inputs drive a state condition in their paired State Generation module that is captured in the State Selection Table.

For example, the Emergency-Mode Network Input is integrated with the Smoke Control Sequencing for UL-864-UUKL State Generation module. The state conditions set by the Emergency-Mode Network Input are Normal, Pressurize, Depressurize, Purge, Shutdown, and Pre-Shutdown. These states are represented in the State Selection Table so that the desired result of the state with the Output Controllers can be set in the table.

The following table describes the Generator Interface Network Input modules and lists the applications in which they are used.

Table 1. Generator Interface Network Input Modules

Name

Description

Applications

APP-MODE

Application Mode - Provides input to the Application Mode Determination State Generation module.

All Air Handling Unit Applications

AUTOCAL-C

Autocalibrate - Provides input to Autocalibration Sequence v50 State Generation module.

All VAV Applications

EHO-MODE

Energy Hold Off Mode - Provides input to Energy Hold Off Determination State Generation module.

EMERGENCY-MODE

Emergency Mode - Provides input to the Smoke Control Sequencing for UL-864-UUKL State Generation module.

OCC-OVERRIDE

Occupancy Override - Provides input to Occupancy Mode Determination State Generation module.

OCC-SCHEDULE

Occupancy Schedule - Provides input to Occupancy Mode Determination State Generation module.

SLINT-S

Sideloop Interlock Status - Provides input to the Sideloop Pass through State Generation module.

SUMWIN-C

SummerWinter - Connects directly to the 2 Pipe Output Control Modules.

SYSTEM-EN

System Enable - Provides input to the Chilled Water System Enable or the Hot Water System Enable State Generation module.

SYSTEM-MODE

System Mode - Provides input to the System Mode Determination State Generation module.

TUNING-RESET

Tuning-Reset - Provides input to the PID Tuning Reset State Generation module used to reset the tuning parameters to the default values present after initial application transfer to the controller.

UNITEN-MODE

Unit Enable Mode - Provides input to Unit Enable Determination State Generation module.

WC-C

WarmupCooldown - Provides input to one of the following modules:

ZNDPR-MODE

Zone Damper Mode - Provides input to the Zone Damper Mode Pass Through SG module.

AHU Multizone (Mixed Air Dual Duct) Applications

ZNHTGVALVE-MODE

Zone Htg Valve Mode - Provides input to the Zone Htg Valve Mode Pass Through SG module.

AHU Multizone (Mixed Air Dual Duct) Applications

ZNSTAGEDHTG-MODE

Zone Staged Htg Mode - Provides input to the Zone Staged Htg Mode Pass Through SG module.

AHU Multizone (Mixed Air Dual Duct) Applications