All Network Inputs with a -EN name are always paired with an Availability type State Generation module. These inputs drive a state condition in their paired State Generation module that is captured in the State Selection Table.
The primary use of the Enable modules is to allow system-wide logic to determine if the Central Heating and Cooling Central Plants are providing Hot or Chilled Water to the devices. For example, if the HTG-EN Network Input is set to a False state, the Box Heating is Available Pass Through State Generation module does not allow the Heating Valve to open on a VAV Box.
The following table describes the Enable Network Input modules and lists the applications in which they are used.
Name |
Description |
Applications |
---|---|---|
BASIN-C |
Drain Basin - Provides input to the Humidification Scrubber Output v51, Output Controller module. |
|
CLG-EN |
Cooling is Available - Provides input to one of the following modules:
|
|
|
||
ECON-EN |
Economizer is Available - Provides an input to the Economizer Availability Determination module. |
|
HC-EN |
2 Pipe is Available - Provides an input to the 2 Pipe is Available Pass Through State Generation module. |
|
HR-EN |
Heat Recovery is Allowed - Allows or locks out Heat Recovery operation where the actual suitability is determined locally to set the device for the heating or cooling operation. |
|
HTG-EN |
Heating is Available and Box Heating is Available - Provides input to one of the following modules:
|
|
|
||
Heating Availability Determination. |
||
HUM-EN |
Humidification is Available - Provides an input to the Humidification is Available Pass Through State Generation module. |
|
PH-EN |
Preheat is Available - Provides an input to the Preheat Availability Determination State Generation module. |
|
RH-EN |
Reheat is Available - Provides an input to the Reheat Availability Determination State Generation module. |
|
SUPHTG-EN |
Supp Heating is Available - Provides an input to the Supplemental Heating is Available Pass Through State Generation module. |
|
SYS-RESET |
System Reset - Provides manual restart functionality. |
|
ZNHTG-EN |
Zone Heating Is Available - Provides input to the Zone Heating Availability Determination State Generation module |