Multistate Value Commands - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

Table 1 describes the Multistate Value object commands. For information about command priorities, see Command Priority Levels.

Table 1. Multistate Value Commands

Name

Description

Operator Override

Replaces Present Value (Appears as O1 for Inputs and I1 for Outputs) at the Operator Override priority with the value you enter in the command. The override has no effect if a higher priority value is in the Present Value attribute.
Note: This command is available only if the Multistate Value is prioritized.

Operator Override Release

Releases an Operator Override command.
Note: This command is available only if the Multistate Value is prioritized.

Release

Releases a specific priority of Present Value (Appears as O1 for Inputs and I1 for Outputs).
Note: This command is available only if the Multistate Value is prioritized.

Release All

Releases Priorities 3 - 15.
Note: This command is available only if the Multistate Value is prioritized.

State 0-N

Releases Priorities 9 - 15 and then writes State 0-N to Present Value (Appears as O1 for Inputs and I1 for Outputs) at Priority 16.
Note: This command is available only if the Multistate Value is prioritized.