Miscellaneous Output Modules - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18
Language
English

The Miscellaneous module category for outputs lists the miscellaneous outputs defined for the system. A miscellaneous output writes to the Stroke Time and Min Pulse of PAO objects.

See the following sections for information:

  • Applications: The application sections list the miscellaneous outputs used by a particular application.

  • Configuring a System: This section explains how to add a miscellaneous output, change a miscellaneous output name, and so on.

  • Commissioning a System: This section explains how to commission miscellaneous outputs.

  • Input and Output Objects: This section describes the objects used in the tool.

See the Upgrading System Files section for a list and description of the module and System Selection changes that were made since the last release of the tool.