Dew Point - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
The Dew Point logic block calculates the dew point temperature of air. The following table describes the inputs and outputs of the Dew Point logic block.

Table 1. Dew Point Block Inputs and Outputs

Name

Data Type

Exposed for Connection by Default

Description

Default Value

Inputs

Dry Bulb Temperature

Float

Yes

Indicates the temperature of air as measured with a simple thermometer.

25 °C, 77 °F

Relative Humidity

Float

Yes

Indicates the relative humidity of air.

50%

Range: 0-100%

Outputs

Dew Point Temperature 1

Float

Yes

Indicates the dew point temperature of air, which is the temperature at which moisture condenses out of the air.

14 °C,

57 °F

Properties

Unit Set

Enum

N/A

Indicates the units of measurement used by the block.

SI, IP

1 This input or output is the Default Element of the block.