Module Use in Application (Add) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The application System Selection trees in the software use the individual modules in the following table.

Table 1. Module Use in Application (Add)

Module Instance Name

Applications

Required CHW Flow Sum

Central Cooling with Optimization Applications

Required CW Flow Sum

Central Cooling with Optimization Applications

Required Tower Flow Sum

Central Cooling with Optimization Applications

Max CHW Flow Sum

Central Cooling with Optimization Applications

Min CHW Flow Sum

Central Cooling with Optimization Applications

Min CW Flow Sum

Central Cooling with Optimization Applications

To see a module's connections and how modules interact with it, view the Connections table.