Reversing Valve Output(s) (HP) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
The Reversing Valve Output selections set the logic in the Staged Compressor Control (Heat Pump Staged Compressors v51) Output module to determine whether the Reversing Valve Outputs (REV1-C and REV2-C) should be commanded on when there is a call for heating or cooling.

The selection options for Reversing Valve Output(s) are:

  • On for Cooling

  • On for Heating