Sensors (FC) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
The selection options for Sensors are:

  • Outdoor Air Temperature: This option provides an optional monitoring point or an input to the Summer Winter Compensation module created under Optional Features (FC).

  • Zone: A Zone Temperature Input is always provided. All the Zone Temperature options assume that a model of the Network Sensor family is being used for Temperature, the Setpoint Adjust options of Common Setpoint Adjust or Warm Cool Adjust, a Temporary Occupancy Interface from the Network Sensor, and the Fan Speed Adjust Option and Humidity input from the Network Sensor. Refer to the Network Sensors product literature to match the functionality selected for the application with a specific Network Sensor hardware model.