Optional Features (FC) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18
Language
English

The Optional Features selections provide Network Inputs modules for Supervisory system interfaces to override the main applications sequence of operation through connections to the appropriate Setpoint/Miscellaneous modules or State Generators.