Fan Status Interlock with Zone Cooling (FC) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
This option is available only if a Stage Cooling Coil is selected. When selected, logic is created to monitor fan status through a binary input. The Airflow Status Determination (Flow Status Determination) module uses this status feedback to enable or disable the Staged Cooling Control (Cooling Staged Outputs v51) Output Controller.