Advanced Dialog Box - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
See the Defining Network Settings (Network Settings Tab) section.

Table 1. Advanced Dialog Box

Field

Description

BACnet Encoding Type

Use to select the file type:

  • Unicode: ISO 10646 (UCS-2)
  • Unicode: ISO 10646 (UTF-8)
  • ASCII: ANSI X3.4 (US-ASCII)
  • Japanese code: Microsoft DBCS code page 932 (Japanese Shift JIS)

By default, BACnet Localization is set to Unicode. Unicode is required when controllers are integrated into a Metasys network. ASCII is required when the controllers are integrated into a Facility Explorer Supervisory Controller. Japanese code is required for Japanese locales.

Baud Rate

Use to select the Baud Rate of Auto, 1200, 9600, 19200, 38400, or 76800. This field is set to Auto by default.

Close

Closes the dialog box and applies the changes.