Field |
Description |
---|---|
System Type |
Specifies the system type. |
Default Controller |
Indicates the default device used when users select the system type in the System Selection wizard.
Note: If you do not have any field controllers on your instance of the Tool, then you must select Artificial Field Device or Artificial IO Device appears as the default controller. The Artificial Field Device allows you to work with an application if you do not have the required hardware packages.
|
Close |
Closes the dialog box. |
|
Opens the Help system. |